Part Number: TMS320C6655
Other Parts Discussed in Thread: SYSBIOS,
Tool/software: Code Composer Studio
Hi TI
I'm using the Code Composer Studio (v6.2.0) together with XDS200 debugger.
I would like to profile a function to verify how many clk cyles it has been used to run through a loop.
By using the "memory browser" I can identify where the function is located in the external RAM and by using asm-file and lst-file I can identify the code start and stop at the memory.
I really need to have a number of clk cyles it has been taken to run through the code.
My setup:
- The C code:
void CpuLoadTask()
{
int i;
RegisterSystemTask((OS_HTask)TSK_SELF());
while (1)
{
if (hPerFunc == NULL)
{
OS_TaskSleep(OS_SECTOTICK(0.1f) );
}
for (i=0 ; i<1000 ; i++)
{
++g_uiCpuLoadDummy;
}
++g_uiCpuLoadCounter;
}
}
- The asm code when the code is loaded into the memory:
CpuLoadTask():
80177120: 01BC54F6 STW.D2T2 B3,*B15--[2]
80177124: 106C6412 CALLP.S2 ti_sysbios_knl_Task_self__E (PC+221984 = 0x801ad440),B3
$C$RL12:
80177128: 1F326592 CALLP.S2 RegisterSystemTask (PC-421076 = 0x8011044c),B3
$C$L8, $C$RL14:
8017712c: 0036B46E LDW.D2T2 *+B14[14004],B0
80177130: 200DA120 [ B0] BNOP.S1 $C$RL16 (PC+26 = 0x8017713a),5
80177134: 1F327293 CALLP.S2 OS_TaskSleep (PC-420972 = 0x801104b4),B3
80177138: 4E26 || MVK.L1 10,A4
$C$L9, $C$RL16:
8017713a: 05A6 MVK.L1 0,A3
8017713c: E8100000 .fphead p, l, W, BU, nobr, nosat, 1000000b
80177140: 0201F42A MVK.S2 0x03e8,B4
80177144: 000C98FA CMPGT.L2X B4,A3,B0
80177148: 3014A120 [!B0] BNOP.S1 $C$L11 (PC+40 = 0x80177168),5
8017714c: 02101FD8 MV.L1X B4,A4
$C$L10:
80177150: 0236B36E LDW.D2T2 *+B14[14003],B4
80177154: 6C6E NOP 4
80177156: 2641 ADD.L2 B4,1,B4
80177158: 0236B37E STW.D2T2 B4,*+B14[14003]
8017715c: E4000000 .fphead n, l, W, BU, nobr, nosat, 0100000b
80177160: 25B0 ADD.L1 A3,1,A3
80177162: 6E08 CMPLT.L1 A3,A4,A0
80177164: CFF8A120 [ A0] BNOP.S1 $C$L10 (PC-16 = 0x80177150),5
$C$L11:
80177168: 0236B26E LDW.D2T2 *+B14[14002],B4
8017716c: 6C6E NOP 4
8017716e: 2641 ADD.L2 B4,1,B4
80177170: 0236B27E STW.D2T2 B4,*+B14[14002]
80177174: 0FE6A120 BNOP.S1 $C$RL14 (PC-52 = 0x8017712c),5
80177178: 00000000 NOP
I would like to profile from addr. 0x8017712c - 0x80177178 to see how many clk cycles it take to run through the code segment.
1. From Code Composer studio I've tried to use: "Tools --> Hardware Trace Analyzer -> Function Profiling --> Trace Range --> Start and Stop Addresses -- > Start Address = 0x80177128 --> Stop Address = 0x80177178 --> Start". But there is no usable result from the trace
I've tried as well:
2. From Code Composer studio I've tried to use: "Tools --> Hardware Trace Analyzer -> Stall Profiling --> Trace Range --> Start and Stop Addresses -- > Start Address = 0x80177128 --> Stop Address = 0x80177178 --> Start". But there is no usable result from the trace as well
Can you please help with a correct guideline.
Thanks
BR
Tam Tran
Vestas Wind System