This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/CC3200-LAUNCHXL: Not able to import and build wlan station example project

Part Number: CC3200-LAUNCHXL

Tool/software: Code Composer Studio

Hi,

I am trying to compile and build wlan station example project as per the youtube video: 

I am using CCS v6.1

But when I import the projects I am getting below errors:

1. An internal error occurred during: "C/C++ Indexer".

assertion failed:

2. Null pointer error: This is when I goto project properties of wlan station.

Please find the attached screenshots also for the errors.

Please help me solve this issue

  • Hi, 

    it looks like an internal CCS error.
    Which CCS version, compiler, TI-RTOS do you use?

    Where you able to build the ti_rtos_config, driverlib and osal projects?

    Restart CCS and try again. 

  • Hi,

    The Release Notes of the SDK version you are using say it was tested with Code composer Studio 8.3 and a newer compiler. In this case, I would strongly suggest you to install this version of CCS in a different directory (so you don't disrupt your current development environment) and retry to import this project. 

    That said, I was able to import the project just fine to my CCSv6.2.0 but I have all the other dependencies already installed as well, thus I suspect it may be an issue with dependencies in your environment. 

    Hope this helps,

    Rafael

  • Hi Rafael,

    I think CCS version was the issue. I installed v7 and everything worked fine.

    Thanks a ton!!