hi all,
my vision sdk version is 0304, kernel version is 4.14, i early boot IPU2 firmware by bootloader, then i run sample_app.out on linux side, but encouter the following assertion:
[HOST] [IPU2 ] 3.412493 s: Assertion @ Line: 706 in utils_stat_collector.c: system_sci_err == SCI_SUCCESS : failed !!!
the error code is SCI_ERR_REVISION, but i have no idea why sci_get_version() return this error of the following code:
if (*plib_func_id != *pmod_func_id)
{
retVal = SCI_ERR_REVISION;
}
if ( pmod_type_id != SC_MOD_TYPE )
{
retVal = SCI_ERR_REVISION;
}
and
i print these values: retVal = -7, *plib_func_id = 1, *pmod_func_id = 0, pmod_type_id = 0x0
could anyone help me figure out this issue?
best regards!