This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I'm running CCS Version: 4.0.2.01003, and there are no updates for it at this time. When creating a new project, it does not have my device variant for MSP430G2231. Where can I obtain this variant?
The downloads are also available here: http://processors.wiki.ti.com/index.php/Download_CCS
Thanks Andy. Upgrading to the latest version of CCS did populate the Device Variant List with the devices I needed. However, the upgrade could not be done through the Help menu of CCS. I had to download the latest version and install it and re-register.
Perhaps some new export licensing requirements had blocked the autoupdate capability in CCS? I had to supply much more registration information then the initial time CCS was installed; it also required the MAC address to my PC. That is one way to assure only one copy of CCS is registered in my name!
Now I can get back to the fun.
P.S. Thanks also to John.