This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/IWR1642BOOST: Building mmWave SDK Demo - 16xx problems

Part Number: IWR1642BOOST
Other Parts Discussed in Thread: MATHLIB

Tool/software: Code Composer Studio

When I try to build the "odsdemo_16xx_dss" file, I am getting the following errors 

Hello team,

I would like to see how the demo of IWR1642BOOST performs, so I downloaded and intsalled the demo, following the guide steps and when the moment of building the project arrived I had some issues:

I fixed a memmory issue and some libraries troubles thanks to your answers to past questions. 

Now I have an error like that:

Compilation failure
subdir_rules.mk:30: recipe for target 'mklib.oe674' failed
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_c_features.h", line 439: warning #48-D: incompatible redefinition of macro "_STLP_VENDOR_CSTD" (declared at line 112 of "C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_c__ti.h")
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s__cstdlib.h", line 103: error #149: declaration is incompatible with builtin "int abs(int)" (declared at line 116 of "C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/stdlib.h")
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s__cstdlib.h", line 103: error #29: expected an expression
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s__cstdlib.h", line 111: error #41: expected an identifier
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s__cstdlib.h", line 111: error #29: expected an expression
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s__cstdlib.h", line 125: error #249: function "abs" has already been defined
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s__cstdlib.h", line 125: error #29: expected an expression
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s__cstdlib.h", line 126: error #41: expected an identifier
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s__cstdlib.h", line 126: error #29: expected an expression
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_manips.h", line 41: warning #78-D: this declaration has no storage class or type specifier
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_manips.h", line 41: error #66: expected a ";"
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_manips.h", line 45: warning #78-D: this declaration has no storage class or type specifier
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_manips.h", line 45: error #66: expected a ";"
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_manips.h", line 48: warning #78-D: this declaration has no storage class or type specifier
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_manips.h", line 48: error #66: expected a ";"
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_manips.h", line 52: warning #78-D: this declaration has no storage class or type specifier
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_manips.h", line 52: error #66: expected a ";"
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_manips.h", line 55: warning #78-D: this declaration has no storage class or type specifier
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_manips.h", line 55: error #66: expected a ";"
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_manips.h", line 58: warning #78-D: this declaration has no storage class or type specifier
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_manips.h", line 58: error #66: expected a ";"
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_manips.h", line 62: warning #78-D: this declaration has no storage class or type specifier
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_manips.h", line 62: error #66: expected a ";"
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_manips.h", line 65: warning #78-D: this declaration has no storage class or type specifier
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_manips.h", line 65: error #66: expected a ";"
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_manips.h", line 69: warning #78-D: this declaration has no storage class or type specifier
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_manips.h", line 69: error #66: expected a ";"
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_manips.h", line 72: warning #78-D: this declaration has no storage class or type specifier
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_manips.h", line 72: error #66: expected a ";"
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_manips.h", line 76: warning #78-D: this declaration has no storage class or type specifier
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_manips.h", line 76: error #66: expected a ";"
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_manips.h", line 79: warning #78-D: this declaration has no storage class or type specifier
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_manips.h", line 79: error #66: expected a ";"
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_manips.h", line 83: warning #78-D: this declaration has no storage class or type specifier
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_manips.h", line 83: error #66: expected a ";"
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_manips.h", line 86: warning #78-D: this declaration has no storage class or type specifier
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_manips.h", line 86: error #66: expected a ";"
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_manips.h", line 90: warning #78-D: this declaration has no storage class or type specifier
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_manips.h", line 90: error #66: expected a ";"
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_manips.h", line 93: warning #78-D: this declaration has no storage class or type specifier
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_manips.h", line 93: error #66: expected a ";"
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_manips.h", line 111: warning #78-D: this declaration has no storage class or type specifier
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_manips.h", line 111: error #66: expected a ";"
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_manips.h", line 114: warning #78-D: this declaration has no storage class or type specifier
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_manips.h", line 114: error #66: expected a ";"
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_manips.h", line 157: warning #78-D: this declaration has no storage class or type specifier
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_manips.h", line 157: error #170: a function type is not allowed here
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_manips.h", line 158: warning #78-D: this declaration has no storage class or type specifier
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_manips.h", line 158: error #66: expected a ";"
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_manips.h", line 160: error #873: "..." is not allowed
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_manips.h", line 160: warning #93-D: identifier-list parameters may only be used in a function definition
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_manips.h", line 162: warning #78-D: this declaration has no storage class or type specifier
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_manips.h", line 162: error #66: expected a ";"
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_manips.h", line 168: warning #12-D: parsing restarts here after previous syntax error
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_manips.h", line 184: warning #78-D: this declaration has no storage class or type specifier
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_manips.h", line 184: error #66: expected a ";"
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_manips.h", line 188: warning #12-D: parsing restarts here after previous syntax error
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_manips.h", line 190: warning #78-D: this declaration has no storage class or type specifier
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_manips.h", line 190: error #66: expected a ";"
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_manips.h", line 194: warning #12-D: parsing restarts here after previous syntax error
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_manips.h", line 197: warning #78-D: this declaration has no storage class or type specifier
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_manips.h", line 197: error #66: expected a ";"
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_manips.h", line 201: warning #12-D: parsing restarts here after previous syntax error
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_manips.h", line 205: warning #78-D: this declaration has no storage class or type specifier
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_manips.h", line 205: error #66: expected a ";"
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_manips.h", line 210: warning #12-D: parsing restarts here after previous syntax error
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_manips.h", line 212: warning #78-D: this declaration has no storage class or type specifier
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_manips.h", line 212: error #66: expected a ";"
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_manips.h", line 217: warning #12-D: parsing restarts here after previous syntax error
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_manips.h", line 226: warning #78-D: this declaration has no storage class or type specifier
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_manips.h", line 226: error #66: expected a ";"
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_manips.h", line 231: warning #12-D: parsing restarts here after previous syntax error
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_traits.h", line 83: warning #78-D: this declaration has no storage class or type specifier
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_traits.h", line 83: error #66: expected a ";"
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_traits.h", line 87: warning #78-D: this declaration has no storage class or type specifier
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_traits.h", line 87: error #66: expected a ";"
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_traits.h", line 91: warning #78-D: this declaration has no storage class or type specifier
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_traits.h", line 91: error #66: expected a ";"
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_traits.h", line 95: warning #78-D: this declaration has no storage class or type specifier
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_traits.h", line 95: error #66: expected a ";"
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_traits.h", line 99: warning #78-D: this declaration has no storage class or type specifier
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_traits.h", line 99: error #66: expected a ";"
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_traits.h", line 103: warning #78-D: this declaration has no storage class or type specifier
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_traits.h", line 103: error #66: expected a ";"
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_traits.h", line 107: warning #78-D: this declaration has no storage class or type specifier
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_traits.h", line 107: error #66: expected a ";"
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_traits.h", line 110: warning #78-D: this declaration has no storage class or type specifier
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_traits.h", line 110: error #66: expected a ";"
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_traits.h", line 113: warning #78-D: this declaration has no storage class or type specifier
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_traits.h", line 113: error #66: expected a ";"
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_traits.h", line 116: warning #78-D: this declaration has no storage class or type specifier
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_traits.h", line 116: error #66: expected a ";"
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_traits.h", line 119: warning #78-D: this declaration has no storage class or type specifier
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_traits.h", line 119: error #66: expected a ";"
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_traits.h", line 122: warning #78-D: this declaration has no storage class or type specifier
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_traits.h", line 122: error #66: expected a ";"
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_traits.h", line 126: warning #78-D: this declaration has no storage class or type specifier
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_traits.h", line 126: error #66: expected a ";"
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_traits.h", line 129: warning #78-D: this declaration has no storage class or type specifier
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_traits.h", line 129: error #66: expected a ";"
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_traits.h", line 133: warning #78-D: this declaration has no storage class or type specifier
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_traits.h", line 133: error #66: expected a ";"
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_traits.h", line 136: warning #78-D: this declaration has no storage class or type specifier
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_traits.h", line 136: error #66: expected a ";"
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_traits.h", line 139: warning #78-D: this declaration has no storage class or type specifier
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_traits.h", line 139: error #66: expected a ";"
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_traits.h", line 143: warning #78-D: this declaration has no storage class or type specifier
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_traits.h", line 143: error #66: expected a ";"
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_traits.h", line 148: warning #78-D: this declaration has no storage class or type specifier
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_traits.h", line 148: error #66: expected a ";"
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_traits.h", line 149: warning #78-D: this declaration has no storage class or type specifier
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_traits.h", line 149: error #66: expected a ";"
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_traits.h", line 155: warning #12-D: parsing restarts here after previous syntax error
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_traits.h", line 157: warning #78-D: this declaration has no storage class or type specifier
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_traits.h", line 157: error #66: expected a ";"
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_traits.h", line 164: warning #12-D: parsing restarts here after previous syntax error
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_traits.h", line 166: warning #78-D: this declaration has no storage class or type specifier
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_traits.h", line 166: error #66: expected a ";"
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_traits.h", line 173: warning #12-D: parsing restarts here after previous syntax error
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_traits.h", line 175: warning #78-D: this declaration has no storage class or type specifier
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_traits.h", line 175: error #66: expected a ";"
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_traits.h", line 178: warning #12-D: parsing restarts here after previous syntax error
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_traits.h", line 223: warning #78-D: this declaration has no storage class or type specifier
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_traits.h", line 223: error #66: expected a ";"
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_traits.h", line 227: warning #78-D: this declaration has no storage class or type specifier
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_traits.h", line 227: error #66: expected a ";"
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_traits.h", line 249: warning #12-D: parsing restarts here after previous syntax error
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_traits.h", line 250: error #20: identifier "__false_type" is undefined
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_traits.h", line 251: error #20: identifier "__false_type" is undefined
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_traits.h", line 259: error #171: expected a declaration
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_traits.h", line 262: warning #78-D: this declaration has no storage class or type specifier
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_traits.h", line 262: error #66: expected a ";"
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_traits.h", line 264: warning #78-D: this declaration has no storage class or type specifier
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_traits.h", line 264: error #66: expected a ";"
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_traits.h", line 267: warning #78-D: this declaration has no storage class or type specifier
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_traits.h", line 267: error #66: expected a ";"
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_traits.h", line 288: warning #78-D: this declaration has no storage class or type specifier
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_traits.h", line 288: error #66: expected a ";"
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_traits.h", line 288: warning #78-D: this declaration has no storage class or type specifier
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_traits.h", line 288: error #66: expected a ";"
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_traits.h", line 288: warning #78-D: this declaration has no storage class or type specifier
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_traits.h", line 288: error #66: expected a ";"
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_traits.h", line 288: warning #78-D: this declaration has no storage class or type specifier
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_traits.h", line 288: error #66: expected a ";"
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_traits.h", line 290: warning #78-D: this declaration has no storage class or type specifier
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_traits.h", line 290: error #66: expected a ";"
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_traits.h", line 290: warning #78-D: this declaration has no storage class or type specifier
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_traits.h", line 290: error #66: expected a ";"
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_traits.h", line 290: warning #78-D: this declaration has no storage class or type specifier
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_traits.h", line 290: error #66: expected a ";"
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_traits.h", line 290: warning #78-D: this declaration has no storage class or type specifier
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_traits.h", line 290: error #66: expected a ";"
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_traits.h", line 292: warning #78-D: this declaration has no storage class or type specifier
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_traits.h", line 292: error #66: expected a ";"
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_traits.h", line 292: warning #78-D: this declaration has no storage class or type specifier
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_traits.h", line 292: error #66: expected a ";"
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_traits.h", line 292: warning #78-D: this declaration has no storage class or type specifier
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_traits.h", line 292: error #66: expected a ";"
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_traits.h", line 292: warning #78-D: this declaration has no storage class or type specifier
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_traits.h", line 292: error #66: expected a ";"
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_traits.h", line 294: warning #78-D: this declaration has no storage class or type specifier
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_traits.h", line 294: error #66: expected a ";"
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_traits.h", line 294: warning #78-D: this declaration has no storage class or type specifier
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_traits.h", line 294: error #66: expected a ";"
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_traits.h", line 294: warning #78-D: this declaration has no storage class or type specifier
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_traits.h", line 294: error #66: expected a ";"
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_traits.h", line 294: warning #78-D: this declaration has no storage class or type specifier
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_traits.h", line 294: error #66: expected a ";"
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_traits.h", line 296: warning #78-D: this declaration has no storage class or type specifier
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_traits.h", line 296: error #66: expected a ";"
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_traits.h", line 296: warning #78-D: this declaration has no storage class or type specifier
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_traits.h", line 296: error #66: expected a ";"
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_traits.h", line 296: warning #78-D: this declaration has no storage class or type specifier
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_traits.h", line 296: error #66: expected a ";"
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_traits.h", line 296: warning #78-D: this declaration has no storage class or type specifier
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_traits.h", line 296: error #66: expected a ";"
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_traits.h", line 299: warning #78-D: this declaration has no storage class or type specifier
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_traits.h", line 299: error #66: expected a ";"
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_traits.h", line 299: warning #78-D: this declaration has no storage class or type specifier
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_traits.h", line 299: error #66: expected a ";"
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_traits.h", line 299: warning #78-D: this declaration has no storage class or type specifier
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_traits.h", line 299: error #66: expected a ";"
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_traits.h", line 299: warning #78-D: this declaration has no storage class or type specifier
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_traits.h", line 299: error #66: expected a ";"
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_traits.h", line 300: warning #78-D: this declaration has no storage class or type specifier
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_traits.h", line 300: error #66: expected a ";"
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_traits.h", line 300: warning #78-D: this declaration has no storage class or type specifier
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_traits.h", line 300: error #66: expected a ";"
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_traits.h", line 300: warning #78-D: this declaration has no storage class or type specifier
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_traits.h", line 300: error #66: expected a ";"
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_traits.h", line 300: warning #78-D: this declaration has no storage class or type specifier
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_traits.h", line 300: error #66: expected a ";"
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_traits.h", line 301: warning #78-D: this declaration has no storage class or type specifier
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_traits.h", line 301: error #66: expected a ";"
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_traits.h", line 301: warning #78-D: this declaration has no storage class or type specifier
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_traits.h", line 301: error #66: expected a ";"
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_traits.h", line 301: warning #78-D: this declaration has no storage class or type specifier
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_traits.h", line 301: error #66: expected a ";"
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_traits.h", line 301: warning #78-D: this declaration has no storage class or type specifier
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_traits.h", line 301: error #66: expected a ";"
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_traits.h", line 302: warning #78-D: this declaration has no storage class or type specifier
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include/s_type_traits.h", line 302: error #66: expected a ";"
Error limit reached.
100 errors detected in the compilation of "C:/ti/ti-cgt-c6000_8.1.3/lib/mklib.c".
Compilation terminated.
gmake[1]: *** [mklib.oe674] Error 1
Building file: "../gen_twiddle_fft32x32.c"
Invoking: C6000 Compiler
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/bin/cl6x" -mv6740 --abi=eabi -O3 --include_path="C:/Users/Xabi/workspace_v9/mmw_dss" --include_path="C:/ti/mmwave_sdk_01_01_00_02/packages" --include_path="C:/ti/mathlib_c674x_3_1_2_1/packages" --include_path="C:/ti/dsplib_c64Px_3_4_0_0/packages/ti/dsplib/src/DSP_fft16x16/c64P" --include_path="C:/ti/dsplib_c64Px_3_4_0_0/packages/ti/dsplib/src/DSP_fft32x32/c64P" --include_path="C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include" -g --gcc --define=SOC_XWR16XX --define=SUBSYS_DSS --define=DOWNLOAD_FROM_CCS --define=DebugP_ASSERT_ENABLED --display_error_number --diag_wrap=off --diag_warning=225 --gen_func_subsections=on --wchar_t=16 --obj_extension=.oe674 --preproc_with_compile --preproc_dependency="gen_twiddle_fft32x32.d_raw" --cmd_file="configPkg/compiler.opt" "../gen_twiddle_fft32x32.c"
Finished building: "../gen_twiddle_fft32x32.c"

Building file: "../gen_twiddle_fft16x16.c"
Invoking: C6000 Compiler
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/bin/cl6x" -mv6740 --abi=eabi -O3 --include_path="C:/Users/Xabi/workspace_v9/mmw_dss" --include_path="C:/ti/mmwave_sdk_01_01_00_02/packages" --include_path="C:/ti/mathlib_c674x_3_1_2_1/packages" --include_path="C:/ti/dsplib_c64Px_3_4_0_0/packages/ti/dsplib/src/DSP_fft16x16/c64P" --include_path="C:/ti/dsplib_c64Px_3_4_0_0/packages/ti/dsplib/src/DSP_fft32x32/c64P" --include_path="C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include" -g --gcc --define=SOC_XWR16XX --define=SUBSYS_DSS --define=DOWNLOAD_FROM_CCS --define=DebugP_ASSERT_ENABLED --display_error_number --diag_wrap=off --diag_warning=225 --gen_func_subsections=on --wchar_t=16 --obj_extension=.oe674 --preproc_with_compile --preproc_dependency="gen_twiddle_fft16x16.d_raw" --cmd_file="configPkg/compiler.opt" "../gen_twiddle_fft16x16.c"
Finished building: "../gen_twiddle_fft16x16.c"

Building file: "../dss_config_edma_util.c"
Invoking: C6000 Compiler
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/bin/cl6x" -mv6740 --abi=eabi -O3 --include_path="C:/Users/Xabi/workspace_v9/mmw_dss" --include_path="C:/ti/mmwave_sdk_01_01_00_02/packages" --include_path="C:/ti/mathlib_c674x_3_1_2_1/packages" --include_path="C:/ti/dsplib_c64Px_3_4_0_0/packages/ti/dsplib/src/DSP_fft16x16/c64P" --include_path="C:/ti/dsplib_c64Px_3_4_0_0/packages/ti/dsplib/src/DSP_fft32x32/c64P" --include_path="C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include" -g --gcc --define=SOC_XWR16XX --define=SUBSYS_DSS --define=DOWNLOAD_FROM_CCS --define=DebugP_ASSERT_ENABLED --display_error_number --diag_wrap=off --diag_warning=225 --gen_func_subsections=on --wchar_t=16 --obj_extension=.oe674 --preproc_with_compile --preproc_dependency="dss_config_edma_util.d_raw" --cmd_file="configPkg/compiler.opt" "../dss_config_edma_util.c"
Finished building: "../dss_config_edma_util.c"

Building file: "../dss_main.c"
Invoking: C6000 Compiler
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/bin/cl6x" -mv6740 --abi=eabi -O3 --include_path="C:/Users/Xabi/workspace_v9/mmw_dss" --include_path="C:/ti/mmwave_sdk_01_01_00_02/packages" --include_path="C:/ti/mathlib_c674x_3_1_2_1/packages" --include_path="C:/ti/dsplib_c64Px_3_4_0_0/packages/ti/dsplib/src/DSP_fft16x16/c64P" --include_path="C:/ti/dsplib_c64Px_3_4_0_0/packages/ti/dsplib/src/DSP_fft32x32/c64P" --include_path="C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include" -g --gcc --define=SOC_XWR16XX --define=SUBSYS_DSS --define=DOWNLOAD_FROM_CCS --define=DebugP_ASSERT_ENABLED --display_error_number --diag_wrap=off --diag_warning=225 --gen_func_subsections=on --wchar_t=16 --obj_extension=.oe674 --preproc_with_compile --preproc_dependency="dss_main.d_raw" --cmd_file="configPkg/compiler.opt" "../dss_main.c"
Finished building: "../dss_main.c"

Building file: "../dss_data_path.c"
Invoking: C6000 Compiler
"C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/bin/cl6x" -mv6740 --abi=eabi -O3 --include_path="C:/Users/Xabi/workspace_v9/mmw_dss" --include_path="C:/ti/mmwave_sdk_01_01_00_02/packages" --include_path="C:/ti/mathlib_c674x_3_1_2_1/packages" --include_path="C:/ti/dsplib_c64Px_3_4_0_0/packages/ti/dsplib/src/DSP_fft16x16/c64P" --include_path="C:/ti/dsplib_c64Px_3_4_0_0/packages/ti/dsplib/src/DSP_fft32x32/c64P" --include_path="C:/ti/ccs910/ccs/tools/compiler/ti-cgt-c6000_8.1.3/include" -g --gcc --define=SOC_XWR16XX --define=SUBSYS_DSS --define=DOWNLOAD_FROM_CCS --define=DebugP_ASSERT_ENABLED --display_error_number --diag_wrap=off --diag_warning=225 --gen_func_subsections=on --wchar_t=16 --obj_extension=.oe674 --preproc_with_compile --preproc_dependency="dss_data_path.d_raw" --cmd_file="configPkg/compiler.opt" "../dss_data_path.c"
gmake[1]: Target 'main-build' not remade because of errors.
gmake: *** [all] Error 2
Finished building: "../dss_data_path.c"

makefile:156: recipe for target 'all' failed

**** Build Finished ****

I would appreciate some help on that.

Best regards. Xavier.

  • Xavier,

    Which version of mmWave SDK are you using? As per this project's Release Notes, it requires SDK version 2.0.0.4.


    If the project is set to use that version of SDK, then it should build without any errors.


    If you do not have that specific version of mmWave SDK installed, you can download and install it from this link.

    Hope this helps.