This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: Code Composer Studio
i am trying to read a text file and write the data in another text file using TM4C123. But I am getting this error
CORTEX_M4_0: Trouble Reading Memory Block at 0x61626280 on Page 0 of Length 0x4: Debug Port error occurred.
CORTEX_M4_0: Trouble Reading Memory Block at 0xbd982000 on Page 0 of Length 0x4: Debug Port error occurred.
I don't know how to solve this error.
Hello Sheetal,
Do you have your TM4C123 connected to your PC via a USB hub? If so, is it a powered hub? There have been similar issues reported for customer who have the device plugged to the PC via a non-powered USB hub. Switching to a powered hub or a direct connection to the PC has helped in that case.
Other common cause is that the the required peripherals have not been enabled when the memory access is attempted. Please make sure they are enabled. Often times the issue occurs because the application did not yet get to the part of the code that enables the peripherals when memory access to specific locations are attempted.
Thanks
ki