Part Number: TMS320F28388D
Other Parts Discussed in Thread: C2000WARE
Tool/software: TI C/C++ Compiler
Tried to run code with sprintf() c28 core:
uint16_t tempBuf[50];
sprintf((char *)tempBuf, "(%.1f) ", 0.1);
Build the project successfully without warning. Stepped into the sprintf(), it failed in __TI_printfi() and jumped to Interrupt_illegalOperationHandler() then freezed.
In project properties, the "Level of printf" is set to "full". The stack size is 4k.
Need some advice. Thanks.