This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: TI C/C++ Compiler
Tried to run code with sprintf() c28 core:
uint16_t tempBuf[50];
sprintf((char *)tempBuf, "(%.1f) ", 0.1);
Build the project successfully without warning. Stepped into the sprintf(), it failed in __TI_printfi() and jumped to Interrupt_illegalOperationHandler() then freezed.
In project properties, the "Level of printf" is set to "full". The stack size is 4k.
Need some advice. Thanks.
Try these two suggestions, in any order.
Formatting floating point numbers is one of the more complicated things sprintf does. Try to format an int.
Since ...
Andy Fung said:The stack size is 4k.
... you probably are not overflowing the stack. But you might be running out of heap. Make the heap larger. Use the linker option --heap_size=number.
Please let me know what happens.
Thanks and regards,
-George
Hello George,
Increase the heap size to 0x1000. However, still having the same issue.
Hello George,
Yes. No problem with formatting an int but failed with float. I need to format a float.
Thanks,
For the source file that calls sprintf, please follow the directions in the article How to Submit a Compiler Test Case. In addition, attach your linker command file to your next post. So the forum will accept it, please add the file extension .txt to it.
Thanks and regards,
-George
Hello George,
Please check the following attached. Thanks.
Building file: "../source.c"
Invoking: C2000 Compiler
"C:/ti/ccs930/ccs/tools/compiler/ti-cgt-c2000_18.12.4.LTS/bin/cl2000" -v28 -ml -mt --cla_support=cla2 --float_support=fpu64 --idiv_support=idiv0 --tmu_support=tmu0 --vcu_support=vcu0 -Ooff --fp_mode=relaxed --fp_reassoc=on --include_path="C:/VEKTREX_TFS/Vektrex/Trunk/SourceCode/ProductSource/WorkSpace_v9_1_28384D/i2c_ex2_eeprom" --include_path="C:/VEKTREX_TFS/Vektrex/Trunk/SourceCode/ProductSource/WorkSpace_v9_1_28384D/i2c_ex2_eeprom/device" --include_path="C:/ti/c2000/C2000Ware_2_01_00_00/driverlib/f2838x/driverlib" --include_path="C:/ti/ccs930/ccs/tools/compiler/ti-cgt-c2000_18.12.4.LTS/include" --advice:performance=all --define=DEBUG --define=CPU1 --printf_support=full --preproc_with_comment --preproc_with_compile --diag_suppress=10063 --diag_warning=225 --diag_wrap=off --display_error_number --gen_func_subsections=on --abi=eabi "../source.c"
Finished building: "../source.c"
MEMORY { /* BEGIN is used for the "boot to SARAM" bootloader mode */ BEGIN : origin = 0x000000, length = 0x000002 BOOT_RSVD : origin = 0x000002, length = 0x0001AE /* Part of M0, BOOT rom will use this for stack */ RAMM0 : origin = 0x0001B0, length = 0x000250 RAMM1 : origin = 0x000400, length = 0x1000//0x0003F8 /* on-chip RAM block M1 */ // RAMM1_RSVD : origin = 0x0007F8, length = 0x000008 /* Reserve and do not use for code as per the errata advisory "Memory: Prefetching Beyond Valid Memory" */ RAMD0 : origin = 0x00C000, length = 0x000800 RAMD1 : origin = 0x00C800, length = 0x000800 RAMLS0 : origin = 0x008000, length = 0x002000 // RAMLS1 : origin = 0x008800, length = 0x000800 // RAMLS2 : origin = 0x009000, length = 0x000800 // RAMLS3 : origin = 0x009800, length = 0x000800 RAMLS4 : origin = 0x00A000, length = 0x000800 RAMLS5 : origin = 0x00A800, length = 0x001800 // RAMLS6 : origin = 0x00B000, length = 0x000800 // RAMLS7 : origin = 0x00B800, length = 0x000800 RAMGS0 : origin = 0x00D000, length = 0x001000 RAMGS1 : origin = 0x00E000, length = 0x001000 RAMGS2 : origin = 0x00F000, length = 0x008000 // RAMGS3 : origin = 0x010000, length = 0x001000 // RAMGS4 : origin = 0x011000, length = 0x001000 // RAMGS5 : origin = 0x012000, length = 0x001000 // RAMGS6 : origin = 0x013000, length = 0x001000 // RAMGS7 : origin = 0x014000, length = 0x001000 // RAMGS8 : origin = 0x015000, length = 0x001000 // RAMGS9 : origin = 0x016000, length = 0x001000 RAMGS10 : origin = 0x017000, length = 0x001000 RAMGS11 : origin = 0x018000, length = 0x001000 RAMGS12 : origin = 0x019000, length = 0x001000 RAMGS13 : origin = 0x01A000, length = 0x001000 RAMGS14 : origin = 0x01B000, length = 0x001000 RAMGS15 : origin = 0x01C000, length = 0x000FF8 // RAMGS15_RSVD : origin = 0x01CFF8, length = 0x000008 /* Reserve and do not use for code as per the errata advisory "Memory: Prefetching Beyond Valid Memory" */ /* Flash sectors */ FLASH0 : origin = 0x080000, length = 0x002000 /* on-chip Flash */ FLASH1 : origin = 0x082000, length = 0x002000 /* on-chip Flash */ FLASH2 : origin = 0x084000, length = 0x002000 /* on-chip Flash */ FLASH3 : origin = 0x086000, length = 0x002000 /* on-chip Flash */ FLASH4 : origin = 0x088000, length = 0x008000 /* on-chip Flash */ FLASH5 : origin = 0x090000, length = 0x008000 /* on-chip Flash */ FLASH6 : origin = 0x098000, length = 0x008000 /* on-chip Flash */ FLASH7 : origin = 0x0A0000, length = 0x008000 /* on-chip Flash */ FLASH8 : origin = 0x0A8000, length = 0x008000 /* on-chip Flash */ FLASH9 : origin = 0x0B0000, length = 0x008000 /* on-chip Flash */ FLASH10 : origin = 0x0B8000, length = 0x002000 /* on-chip Flash */ FLASH11 : origin = 0x0BA000, length = 0x002000 /* on-chip Flash */ FLASH12 : origin = 0x0BC000, length = 0x002000 /* on-chip Flash */ FLASH13 : origin = 0x0BE000, length = 0x002000 /* on-chip Flash */ CPU1TOCPU2RAM : origin = 0x03A000, length = 0x000800 CPU2TOCPU1RAM : origin = 0x03B000, length = 0x000800 CPUTOCMRAM : origin = 0x039000, length = 0x000800 CMTOCPURAM : origin = 0x038000, length = 0x000800 CANA_MSG_RAM : origin = 0x049000, length = 0x000800 CANB_MSG_RAM : origin = 0x04B000, length = 0x000800 RESET : origin = 0x3FFFC0, length = 0x000002 } SECTIONS { codestart : > BEGIN .text : >> RAMGS2//RAMD0 | RAMD1 | RAMLS0 | RAMLS1 | RAMLS2 | RAMLS3 .cinit : > RAMM0 | RAMGS2 .switch : > RAMM0 | RAMGS2 .reset : > RESET, TYPE = DSECT /* not used, */ .stack : > RAMM1 .heap : > RAMM1 #if defined(__TI_EABI__) .bss : > RAMLS0 | RAMLS5 | RAMGS2 .bss:output : > RAMLS0 | RAMGS2 .init_array : > RAMM0 | RAMGS2 .const : > RAMLS5 | RAMGS2 .data : > RAMLS5 | RAMGS2 .sysmem : > RAMLS4 | RAMGS2 #else .pinit : > RAMM0 .ebss : >> RAMLS5 //| RAMLS6 .econst : > RAMLS5 .esysmem : > RAMLS5 #endif ramgs0 : > RAMGS0, type=NOINIT ramgs1 : > RAMGS1, type=NOINIT MSGRAM_CPU1_TO_CPU2 > CPU1TOCPU2RAM, type=NOINIT MSGRAM_CPU2_TO_CPU1 > CPU2TOCPU1RAM, type=NOINIT MSGRAM_CPU_TO_CM > CPUTOCMRAM, type=NOINIT MSGRAM_CM_TO_CPU > CMTOCPURAM, type=NOINIT RAMLS5_VAR > RAMLS5, type=NOINIT /* The following section definition are for SDFM examples */ // Filter_RegsFile : > RAMGS0 // Filter1_RegsFile : > RAMGS1, fill=0x1111 // Filter2_RegsFile : > RAMGS2, fill=0x2222 // Filter3_RegsFile : > RAMGS3, fill=0x3333 // Filter4_RegsFile : > RAMGS4, fill=0x4444 // Difference_RegsFile : >RAMGS5, fill=0x3333 .TI.ramfunc : {} > RAMGS2//RAMM0 } /* //=========================================================================== // End of file. //=========================================================================== */
Hello
You're correct in allocating additional memory for stack and heap.
However, it looks you've only made that adjustment in CCS and not in the linker command file. Currently your stack and heap share 0x1000 words.
Update your linker command file to link the stack and heap sections to a larger memory section (maybe a RAMGSx).
Best regards
Chris
Hello Chris,
I updated the stack and heap size in the linker command file. You could see that in my attached cmd file.
Thanks,
Andy,
I don't see your attachment. Did this resolve your issue?
Best regards
Chris
Andy
Yes, I reviewed that linker. It is only allocating 0x1000 words to stack and heap (which they are sharing).
You need to update your linker command file to link the stack and heap sections to a larger memory section (maybe a RAMGSx).
Best regards
Chris
Hello Chris,
I updated the cmd file like this:
.heap : > RAMM1 | RAMGS11 | RAMGS12 | RAMGS13
.stack : > RAMM1 | RAMGS11 | RAMGS12 | RAMGS13
Each of which has 0x1000. However, I am still having the same issue.
Thanks,
Andy,
Not sure if this fixes the issue, it will be better to test with a combined section.
Similar to how RAMLS0 in your linker combines LS0 to LS3, I'd like you to combine either some RAMLSx or lower GS rams such RAMGS0/1/2 so that you have at least 0x2000 words. A stack and heap of 0x1000 each should be enough.
Assign this combined memory section to .heap and .stack to see if that fixes it.
Best regards
Chris
Hello Chris,
I updated the cmd file as below and the sprintf is working now. The RAMLS0 is combined with RAMLS2 /RAMLS3 /RAMLS4 /RAMLS5
RAMLS0 : origin = 0x008000, length = 0x3000
.heap : > RAMLS0
.stack : > RAMLS0
I tried similar thing with RAMGSx. Combined RAMGS6 / RAMGS7 / RAMGS8 / RAMGS9 / RAMGS10 but it doesn't work. What is the reason of that?
Thanks
Andy,
Great!
My guess on why that doesn't work is that the stack space is beyond the lower 64k words.
Best regards
Chris