This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS: How to modify the size of C71 L2 cache?

Tool/software: Code Composer Studio

Hi,

    In psdk_rtos_auto_j7_06_02_00_21/vision_apps, the C71 L2 cache configured to 32KB.

    I want to set all L2(512KB) to cache, what should I do?

thanks.

  • Can you try changing the value to 512KB?

    vision_apps/apps/basic_demos/app_tirtos/tirtos_linux/c7x_1/c7x_1.cfg

    Cache.initSize.l2Size  = Cache.L2Size_512K;

    Also 448KB is configured as L2 SRAM so you will have move that space to DDR,

    vision_apps/apps/basic_demos/app_tirtos/tirtos_linux/c7x_1/linker.cmd

        .bss:l2mem              (NOLOAD)(NOINIT) : {} > DDR_C7x_1 /*L2RAM_C7x_1*/

    Regards,
    Shyam

  • Hi,

        Thanks for your reply.

        I had changing the value to 512KB base on your advise, but the performance of our project have no change.

        Can you tell me, how to check the L2 cache size after config?

    Thanks.

  • Hi,

    L2 cache size control register which has the L2 size.