This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/AWR6843: driver vital sign monitoring

Part Number: AWR6843
Other Parts Discussed in Thread: AWR1642, UNIFLASH, , IWR6843ISK-ODS, IWR6843ISK

Tool/software: Code Composer Studio

Dear sir or madam,

I want to know if you can implement driver vital sign with AWR6843 ( that's just this lab example from AWR6843:  dev.ti.com/.../node
can you use the .bin program from AWR1642 for AWR6843,
you have to change all the code or there is a conversion for code from AWRs?

best regards

Alireza

  • Hi Alireza,

    The lab you referred to in your post already supports AWR6843 as mentioned in the lab user guide. It provides separate pre-compiled binaries as well as CCS projects for all the supported devices listed in the lab user guide. You will need to use the pre-compiled binary corresponding to xWR6843 available at the following path: mmwave_automotive_toolbox_3_0_0\labs\lab0003_occupancy_detection\prebuilt_binaries\oddemo_68xx.bin

    If you are looking for the Vital signs demo for xWR6843, it is available in the Industrial Toolbox as given below:

    xWR6843 Vital Signs Lab: http://dev.ti.com/tirex/explore/node?node=ADTLXelX36I6iOJjRnxYYA__VLyFKFf__LATEST

    Binaries from xWR1642 are not compatible with xWR6843 because these devices are based on different RF frequencies, however you can follow the instructions given in the following migration guide to post xWR1642 software to xWR6843 (60GHz) or xWR1843 (77GHz). As mentioned above, the Vital Signs Demo is already available for xWR6843 in the Industrial Toolbox.

    Link to MIgration Guide: Migrating to xWR68xx and xWR18xx Millimeter Wave (Rev. B)

    Regards

    -Nitin 

      

  • Hi Nitin,

    thank you very much for your answer. I can use IWR6843ISK Antenna Module or IWR6843ISK-ODS Antenna Module  for  Vital Signs Driver Demo. Can i use AWR6843ISK EVM for this case? I have problem with UNIFlash program. I can't find any AWR6843ISK EVM, if i search this name, i can only find AWR6843 and not EVM.

    Thank you very much

    best regards 

    Alireza

  • Hi Alireza,

    1. I can use IWR6843ISK Antenna Module or IWR6843ISK-ODS Antenna Module  for Vital Signs Driver Demo.

    [NS]: Not sure if this was a question (or a statement), but yes the Vital signs demo can work on both IWR6843ISK or IWR6843ISK-ODS modules.

    2. Can i use AWR6843ISK EVM for this case? I have problem with UNIFlash program. I can't find any AWR6843ISK EVM, if i search this name, i can only find AWR6843 and not EVM.

    Just select AWR6843 in uniflash and it should be OK.

    Let us know if you see any issues.

    Regards

    -Nitin