This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

After import of project, CCSv4 will only do a clean build

I had a computer crash and lost the ability to load my workspace. I created a new workspace and imported my project. I didn't see any errors associated with the import but I am unable to build my project. Whether I select "clean", "build active project", "rebuild active project", etc... It always just does a clean build

 

**** Clean-only build of configuration F2833x_RAM for <my project name> *****

I then get a bunch of errors that files can't be found. But that is normal since this is a new project workspace and there are no files to clean yet.

It ends with "Build complete for project <project name>"

But nothing is built since it is a clean build.

Any ideas on how to get CCSv4 to actually build my project?

 

I am running version: 4.2.1.00004 

Thanks

  • Does this issue only occur with this specific project and not others? If so, could you attach your project here so we can check if we can reproduce the issue at our end?

  • Hello Aarti!

    I only tried importing one. It is the main project I am working on at the moment. I gave up trying to get the imported project to work so I created a new project and manually recreated the project. Ufortunately I have deadlines coming up so I could not mess with it anymore. I had to move on.

     

    Thanks

     

  • MaxPower said:
    Ufortunately I have deadlines coming up so I could not mess with it anymore. I had to move on.

    I understand. I'm sorry we couldn't get to the bottom of the issue, but if you do run into the issue again or still have access to the old project, feel free to zip it up and attach it at a later time.