This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I am attempting to create a multi branch pipeline in Jenkins to do continuous integration of our CCS builds.
In my Jenkinsfile, I would like to use the following line to create a workspace on the fly via importing a valid CCS project that is in the base directory of the new workspace.
org.eclipse.core.internal.resources.ResourceException: Invalid project description. at org.eclipse.core.internal.resources.Project.checkDescription(Project.java:173) at org.eclipse.core.internal.resources.Project.assertCreateRequirements(Project.java:57) at org.eclipse.core.internal.resources.Project.create(Project.java:266) at org.eclipse.core.internal.resources.Project.create(Project.java:252) at com.ti.ccstudio.project.core.services.ProjectImporter.internalImportProject(ProjectImporter.java:468) at com.ti.ccstudio.project.core.services.ProjectImporter.access$1(ProjectImporter.java:415) at com.ti.ccstudio.project.core.services.ProjectImporter$1.run(ProjectImporter.java:377) at org.eclipse.core.internal.resources.Workspace.run(Workspace.java:2292) at org.eclipse.core.internal.resources.Workspace.run(Workspace.java:2317) at com.ti.ccstudio.project.core.services.ProjectImporter.importProject(ProjectImporter.java:375) at com.ti.ccstudio.project.core.services.ProjectImporter.importProject(ProjectImporter.java:340) at com.ti.ccstudio.apps.internal.project.ProjectImportApp.doRun(ProjectImportApp.java:169) at com.ti.ccstudio.apps.internal.BaseHeadlessApp$1.run(BaseHeadlessApp.java:338) at org.eclipse.core.internal.resources.Workspace.run(Workspace.java:2292) at org.eclipse.core.internal.resources.Workspace.run(Workspace.java:2317) at com.ti.ccstudio.apps.internal.BaseHeadlessApp.internalRun(BaseHeadlessApp.java:336) at com.ti.ccstudio.apps.internal.BaseHeadlessApp.start(BaseHeadlessApp.java:258) at org.eclipse.equinox.internal.app.EclipseAppHandle.run(EclipseAppHandle.java:203) at org.eclipse.core.runtime.internal.adaptor.EclipseAppLauncher.runApplication(EclipseAppLauncher.java:137) at org.eclipse.core.runtime.internal.adaptor.EclipseAppLauncher.start(EclipseAppLauncher.java:107) at org.eclipse.core.runtime.adaptor.EclipseStarter.run(EclipseStarter.java:401) at org.eclipse.core.runtime.adaptor.EclipseStarter.run(EclipseStarter.java:255) at sun.reflect.NativeMethodAccessorImpl.invoke0(Native Method) at sun.reflect.NativeMethodAccessorImpl.invoke(Unknown Source) at sun.reflect.DelegatingMethodAccessorImpl.invoke(Unknown Source) at java.lang.reflect.Method.invoke(Unknown Source) at org.eclipse.equinox.launcher.Main.invokeFramework(Main.java:657) at org.eclipse.equinox.launcher.Main.basicRun(Main.java:594) at org.eclipse.equinox.launcher.Main.run(Main.java:1465)
Hello, If I understand correctly:
You create a new folder in the filesystem that has a valid CCS project in it. You then wish to use that new folder as a workspace folder and import the project that physically resides in the folder to the workspace.
Is that correct? If so:
Wesley C said:C://ti/ccs1020/ccs/eclipse/eclipsec.exe -noSplash -application com.ti.ccstudio.apps.projectImport -data %WORKSPACE% -ccs.location %WORKSPACE%
The above command should work except for the last parameter. -ccs.location needs the path to the project folder itself. So I would expect something like:
-ccs.location %WORKSPACE%/myproject
Please see if that helps.
Thanks
ki