Other Parts Discussed in Thread: TM4C1294NCPDT
The attached example for a TM4C1294NCPDT creates initialised sections which contain holes, due use of a section placed at a specific address:
$ ~/ti/ccs1020/ccs/tools/compiler/ti-cgt-arm_20.2.4.LTS/bin/armofd --xml TM4C1294NCPDT_fixed_checksum.out | ~/ti/ti-processor-sdk-rtos-am335x-evm-05.01.00.11/cg_xml/bin/sectti
Reading from stdin ...
************************************************************
REPORT FOR FILE: TM4C1294NCPDT_fixed_checksum.out
************************************************************
Name : Size (dec) Size (hex) Type Load Addr Run Addr
-------------------- : ---------- ---------- ---- ---------- ----------
.intvecs : 520 0x00000208 DATA 0x00000000 0x00000000
.text : 68 0x00000044 CODE 0x00000208 0x00000208
.stack : 512 0x00000200 UDATA 0x20000000 0x20000000
.TI.bound:CHECKSUM : 2 0x00000002 DATA 0x000f0000 0x000f0000
------------------------------------------------------------
Totals by section type
------------------------------------------------------------
Uninitialized Data : 512 0x00000200
Initialized Data : 522 0x0000020a
Code : 68 0x00000044
Due to the holes the expected binary file size is 0xF0002 = 983042.
The attached example has two ways of generating a binary output file:
- A post-build rule using armobjcopy from the TI ARM v20.2.4 compiler
- armhex from the TI ARM v20.2.4 compiler, configured using the CCS project properties under CCS Build -> Arm Hex Utility. The only options set were the output format (set to --binary) and the output filename (--outfile).
The complete output from the CCS build console, including the two methods to create binary output files:
**** Build of configuration Debug for project TM4C1294NCPDT_fixed_checksum ****
/home/mr_halfword/ti/ccs1020/ccs/utils/bin/gmake -k -j 12 all -O
Building file: "../main.c"
Invoking: Arm Compiler
"/home/mr_halfword/ti/ccs1020/ccs/tools/compiler/ti-cgt-arm_20.2.4.LTS/bin/armcl" -mv7M4 --code_state=16 --float_support=FPv4SPD16 -me --include_path="/home/mr_halfword/workspace_v10/TM4C1294NCPDT_fixed_checksum" --include_path="/home/mr_halfword/ti/ccs1020/ccs/tools/compiler/ti-cgt-arm_20.2.4.LTS/include" --define=ccs="ccs" --define=PART_TM4C1294NCPDT -g --gcc --diag_warning=225 --diag_wrap=off --display_error_number --abi=eabi --asm_listing --preproc_with_compile --preproc_dependency="main.d_raw" "../main.c"
Finished building: "../main.c"
Building file: "../tm4c1294ncpdt_startup_ccs.c"
Invoking: Arm Compiler
"/home/mr_halfword/ti/ccs1020/ccs/tools/compiler/ti-cgt-arm_20.2.4.LTS/bin/armcl" -mv7M4 --code_state=16 --float_support=FPv4SPD16 -me --include_path="/home/mr_halfword/workspace_v10/TM4C1294NCPDT_fixed_checksum" --include_path="/home/mr_halfword/ti/ccs1020/ccs/tools/compiler/ti-cgt-arm_20.2.4.LTS/include" --define=ccs="ccs" --define=PART_TM4C1294NCPDT -g --gcc --diag_warning=225 --diag_wrap=off --display_error_number --abi=eabi --asm_listing --preproc_with_compile --preproc_dependency="tm4c1294ncpdt_startup_ccs.d_raw" "../tm4c1294ncpdt_startup_ccs.c"
Finished building: "../tm4c1294ncpdt_startup_ccs.c"
Building target: "TM4C1294NCPDT_fixed_checksum.out"
Invoking: Arm Linker
"/home/mr_halfword/ti/ccs1020/ccs/tools/compiler/ti-cgt-arm_20.2.4.LTS/bin/armcl" -mv7M4 --code_state=16 --float_support=FPv4SPD16 -me --define=ccs="ccs" --define=PART_TM4C1294NCPDT -g --gcc --diag_warning=225 --diag_wrap=off --display_error_number --abi=eabi --asm_listing -z -m"TM4C1294NCPDT_fixed_checksum.map" --heap_size=0 --stack_size=512 -i"/home/mr_halfword/ti/ccs1020/ccs/tools/compiler/ti-cgt-arm_20.2.4.LTS/lib" -i"/home/mr_halfword/ti/ccs1020/ccs/tools/compiler/ti-cgt-arm_20.2.4.LTS/include" --reread_libs --diag_wrap=off --display_error_number --warn_sections --xml_link_info="TM4C1294NCPDT_fixed_checksum_linkInfo.xml" --rom_model -o "TM4C1294NCPDT_fixed_checksum.out" "./main.obj" "./tm4c1294ncpdt_startup_ccs.obj" "../tm4c1294ncpdt.cmd" -llibc.a
<Linking>
Finished building target: "TM4C1294NCPDT_fixed_checksum.out"
Building files: "TM4C1294NCPDT_fixed_checksum.out"
Invoking: Arm Hex Utility
"/home/mr_halfword/ti/ccs1020/ccs/tools/compiler/ti-cgt-arm_20.2.4.LTS/bin/armhex" --diag_wrap=off --binary -o "TM4C1294NCPDT_fixed_checksum.armhex_bin" "TM4C1294NCPDT_fixed_checksum.out"
Translating to Binary format...
"TM4C1294NCPDT_fixed_checksum.out" .intvecs ==> .intvecs
"TM4C1294NCPDT_fixed_checksum.out" .text ==> .text
"TM4C1294NCPDT_fixed_checksum.out" .TI.bound:CHECKSUM ==> .TI.bound:CHECKSUM
Finished building: "TM4C1294NCPDT_fixed_checksum.out"
Create binary file
/home/mr_halfword/ti/ccs1020/ccs/tools/compiler/ti-cgt-arm_20.2.4.LTS/bin/armobjcopy -O binary TM4C1294NCPDT_fixed_checksum.out TM4C1294NCPDT_fixed_checksum.objcopy_bin
**** Build Finished ****
The size of the generated binary files are:
$ ls -l *bin*
-rw-rw-r-- 1 mr_halfword mr_halfword 590 Apr 2 10:15 TM4C1294NCPDT_fixed_checksum.armhex_bin
-rw-rw-r-- 1 mr_halfword mr_halfword 983042 Apr 2 10:15 TM4C1294NCPDT_fixed_checksum.objcopy_bin
The binary file created by armobjcopy has the expected size.
However, the binary file created by armhex is just the total size of all the initialised sections. I.e. not a valid binary file since has excluded the holes between the initialised sections. Looking at the ARM Assembly Language Tools v20.2.0.LTS User's Guide using a combination of --binary and --image along with a ROMS directive would allow a valid binary file to be created in this case.
Is it a bug in armhex that just using the --binary option can cause the output file to not contain the holes between the initialised sections?