This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

TIDA-00774: Off the shelf options

Prodigy 30 points

Replies: 1

Views: 358

Part Number: TIDA-00774

Hi,

Before I begin creating one of these from scratch, do you know if there are already assembled kits or something similar off the shelf? Not looking to develop or modify any of the design. I just need to drive a BLDC motor at 200W continuous. 

Thanks,

Blake

  • Hi Blake,

    Good to see that you are referring TIDA-00774. These are reference designs solving specific problems, and we don't make them in bulk. I am sorry to say that I don't have any, off the shelf board which I can ship. I think you need to make your own board using the resources available from http://www.ti.com/tool/TIDA-00774

    Thanks,

    Manu

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.