What benefits does the “smooth transition” feature offer in the implementation of Power over Ethernet (PoE) Powered Device (PD)?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
What benefits does the “smooth transition” feature offer in the implementation of Power over Ethernet (PoE) Powered Device (PD)?
The PMP20859 is a Dual-input redundant PoE PD reference design with the smooth transition feature. The smooth transition feature enables the delivery of non-interrupted output power. The PMP20859 reference design accepts two IEEE802.3bt inputs and an auxiliary input from a wall adapter. As long as one input remains connected, the other two inputs can be disconnected and/or reconnected without any interruption to the 5V/6A output power.
To learn more about the performance of this reference design under typical and stress test conditions, refer to section 2 "Testing and Results" of the User Guide for PMP208959.
You can also download the design files (BOM, Schematic, Gerber) for this reference design from the PMP20859 folder.