Other Parts Discussed in Thread: TPA3110D2, LM5122
Hi
In the reference design( pdf file name : tidras4 ) there are five 0.009 resistors(R42-R46) kept in between the output of Boost converter (LM5122M) and the class D Power amplifier.(TPA3110D2). But there is no mention of the same in the BOM.Could you please share the specification of the same?
Also what is the purpose of these resistors ? Can we connect the output of the boost converter directly to the Class D power supply input.
In our automotive application we are using 24V battery as the input to boost converter. please suggest any changes required.? We are using TPA3118 class D amplifier instead of TPA3110D2