Hello
i have a question.
At present, each switch of Control Card is ON / OFF as shown in the picture.
A yellow arrow pointing up means the switch is up, and a down arrow means the switch is down.
I want to program TIDA-01604 without USB 5V power.
In other words, I want to BOOT with flash memory.
To boot to flash memory, read the datasheet and circuit diagram. You need to give S1 switch to GPIO24 and GPIO32 without any other configuration or setting.
In the picture I sent you, let me know if you have to put both S1 switches up or down.
S1: I would appreciate it if you let me know.