Part Number: TIDA-010071
Hi,
We were thinking of using TIDA-00637 for a project, but I see that TIDA-010071 has been released in 2019 whereas TIDA-00637 has been released in 2015.
Are there any circumstances under which we shouldn't use the latest design? (TIDA-010071)
To be a little more specific, we're working on an IoT application, and I note that TIDA-010071 doesn't seem to have an microcontroller, but TIDA-00637 has a MSP430 MCU. So can TIDA-010071 still be used somehow with a WiFi module, like CC3120?
I also wanted to know if it is wise to consider using TIDC-EVSE-WIFI, since it was also released a while ago (2016).
Any input is appreciated. Thanks!