Other Parts Discussed in Thread: BQ76940, BQ34Z100, BQ34Z100-G1
Hello forum,
I am reviewing TIDA-010030 design. I want to customize this design parameters for me. Want to increase current ratings for example IDSCH: 80 ~90 A. For this value I made some calculations for current thresholds. There are some threshold values in below for bq76940 and bq34z100.
CCrange: -+200 mV CCfull :-+270 mV OCDrange: 8~100 mV SCDrange: 22~200 mV Vsr(bq34z100) : -+125 mV
One of the most important thing is that can I find a sense resistor in market. For this limitations I decided to choose 1m ohm equivelent sense resistor value (three 3R or two 2R in parallel).And I assign a value for design marjin as %10. All of values above will decrease %10 in below calculations.
**For SCD calculation -> I-SCDmax = VSCD * Rsense = 180m * 1m = 180A
**For OCD calculation -> I-OCDmax = VOCD * Rsense = 90m * 1m = 90A
**For CCrange control -> I took I-DSCmax = 80A -> -> -> V-CCSR = I-DSCmax * Rsense = 80 * 1m = 80 mV
There is no problem for now as it seems. My question is in below actually.
**For bq34z100 Vsr range control which is the right selection? -> Vsr(bq34z100) / I-SCDmax or Vsr(bq34z100) / I-OCDmax
GOOD DAYS AND JOBS
EMRE