Other Parts Discussed in Thread: UCC21540, TIDA-01604
Dear TI Team,
I have a requirement for 3Phase inverter 27KW! for which I was planning to use your reference design TIDA-020030 connecting 3 of them 1 for each phase.
My technical requirement is as below:
Sr No. | Parameter | Specification |
1 | Rated output | 25 kW at 0.8 PF lagging |
2 | Load | 25kW load comprises of 5.5kW and 2.2kW motor load respectively. Both the inductive loads are connected to inverter through individual Soft Starters. When the motor loads are not running, Inverter is supposed to run on 25kW load with continuous duty. Also, Inverter should be designed to withstand sudden loading from 0-100%. |
3 | Input supply (DC) | 20V to 50V. Functional range should be from 24-33V DC, whereas it should be able to withstand upto 50V and enable disconnection incase voltage rises above 33V. |
4 | Output supply (AC) | 415V, 50HZ, 3PH. Tolerances: Voltage : ± 1.5% Frequency : ± 2% |
5 | Efficiency | >90% |
6 | Over load rating | 110% for 30 minutes |
7 | Duty | Continuous. Frequent motor operations are envisaged. |
8 | Harmonics | Overall : less than 5% Individual : 3% Input ripple : <3% |
So what changes do i need to do? Do you suggest to use DC DC converter to boost the I/P voltage. If so could you suggest me any TI reference design for the same? Deeply awaiting your reply and thanks in advance.
Regards,
Vijay Gohil