Other Parts Discussed in Thread: UCC2897A
Hi all
what is "ERROR(ORPSIM-16296): Invalid Expression: Specify either current(I) or voltage(V)."
Is there an established circuit that contains ACF Forward and IC UCC2897A ,Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi all
what is "ERROR(ORPSIM-16296): Invalid Expression: Specify either current(I) or voltage(V)."
Is there an established circuit that contains ACF Forward and IC UCC2897A ,Thanks.
Micky,
Thanks for your interest in UCC2897A and TI here. Can you attach your simulation file? I'll assign to an apps engineer to support your questions.
Regards,
John
Hi John,
This is the file I downloaded. Can I modify this file to the voltage and current I want?
Thanksslum429.zip
Hi,
You can modify either voltage or current but if your modification is outside of the existing design can do then you need to modify associated component values together.
Hi Hong,
OK, in addition, is there a way to modify the simulation time, or can I close the values that do not need to be displayed, because the simulation time is too long,
Thanks
Hi,
Yes, you can do these. You need to follow what PSpice instructions how to do them.
Hi Hong,
But he didn't let me modify the simulation time, it seems to be locked, can I provide more detailed information,
Thanks
Hi,
You need to save the project to a new one, such as to a new folder from PSprice. Then you can change the simulation time.
Hi Hong,
OK, I will try it.
May I only display the voltage and current of the installed probe, and not display the other ones that are not installed, so that the simulation can run faster.
Thanks
Hi Hong,
Where should I set up? Is it set from Simulation Setting? Is there a more detailed explanation,
Thanks
Hi Hong,
I follow your way and modify the circuit diagram. No matter how you change it, the output is the same as the original one. I wonder if it is still locked and the simulation results have not changed.
Thanks
You can create your folder anywhere on your computer. After create a new folder then open pspice and follow the steps I described.
Hi Hong
I modified the feedback resistance value and the switching frequency resistance setting of the IC, but my Mosfet did not work, resulting in no output voltage. May I ask which part of the problem might be wrong.
Thanks
Hi,
If before modifying the circuit can work and after modifying cannot, the issue is on your modifying or on your Pspice setup. You would have to figure out where is wrong.
I suggest you use the original MOSFETS to make simulation. If new MOSFETS cannot work you need to talk to your MOSFET provider.
Another is your simulation setup but that has to be on your debugging for example if your simulation time is too short.