Hello team,
I received a question from my customer about Buck/boost controller. I would appreciate if you could give us some advice about it.
The customer is willing to use a buck/boost controller for their system and thought that PMP21278 would have the closest specification for their system. But the max output current is 25A and their requirement is 30A.
I believe that this 25A is related to heat, but can they operate it up to 30A if they take any measures? If yes, what should they change? And if that is not possible, I would appreciate if you could tell me a recommended circuit that could be used instead.
Best Regards,
Ryotaro Fukui