Other Parts Discussed in Thread: TINA-TI
Hi,
I created a simple transformer circuit in TINA-TI using the spice model downloaded from TDK website ALT4532M-201-T001 : Detailed Information | Transformers - Pulse Transformers and Modules for LAN | TDK Product Center. Attached is the circuit schematics from TINA-TI. The same link also has a .pdf file describing the circuit used for the spice model.
AC Transfer Characteristics seems to run fine along with some of the other analyses. However, transient simulation terminates with a Floating Point Overflow Error right at the start. Can someone please help to identify if this is due to an error in the SPICE model, or an issue with TINA simulator or if I need to change some TINA simulation parameter settings for it to run successfully?
I can run transient simulation fine of much more elaborate circuits using TI opamp models on TINA-TI. I think I am using the latest version of the simulator: Version 9.3.200.277 SF-TI
Thanks,
Satish