This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PMP7233: Simulator for automotive cranking pulses evaluation module -AUTOCRANKSIM-EVM (HVL068A)

Part Number: PMP7233

Hi Team,

 

Currently, we plan to use AUTOCRANKSIM-EVM (HVAL068A)

Here I attached the waveform which we want to generate from it.

 

Questions:

Can It generate the attached waveform or suggest another solution for generating the waveform?

As per our attached waveform & Voltage range.
Required Output Voltage range is 2 to 28.5V dc.
Please confirm Out voltage range of EVM: AUTOCRANKSIM-EVM (HVAL068A).
In User guide “HVL068A Cranking Simulator User's Guide”
Output Voltage range is 2 V to 15 V dc.
Can we change it? Please give suggestions for it.

please provide prices & Delivery period.