Other Parts Discussed in Thread: LM5022, TL431, TL431LI
Hi,
I'm a student in electronics and for a project i made an exact copy of the reference design PMP20588.
After soldering I fail to get any voltage after the transfo.
Some measerments:
Uvlo = 3,1V
Vin = 24,1 V
Vsec of transfo = 0V
Voltage across the mosfet is also 24 V so it won't switch.
I didn't soldered R4 yet to ensure i have a correct voltage before i go further with the network stuff.
Thank you for your help
Willem