This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PMP10215: L8 & L9 in schematic don't match BOM parts

Part Number: PMP10215

Hi there, I am finally assembling our make of the PMP10215 Evaluation Board and have ordered inductors L8 & L9 as per Rev D (and Rev E) BOM's from the TI website.  I've just realised that in the BOM it specifies the use of Wirth 744741101 inductors which are actually 100uH not the 10uH that the schematic shows.  Will it be a problem using the 100uH inductors that I have purchased?  If so, which part is the correct value for inductors L8 & L9?

Thank you.

Mark