Other Parts Discussed in Thread: EV2400, , BQ76930
HI ,
Please check attached video of EV2400 GUI reader from Texas Instruments.
I tried to read Bq7693006dbt AFE which is for 10 cells of my custom Hardware , which i made using reference of TIDA-01093 Design.
U all can go through the Video attached here.
I made cell 4 and cell 9 short to make it 8S.
At times readings are correct and at times they are incorrect like what given in video.
Also consider a case when BMS Board is fully Power OFF and voltage sensing connections are removed and reconnected , across RC filter of AFE i mean across capacitor for example Cell no 5 capacitor shows 5 / 6 volts and cells adjacent to it shows lesser value around 0.2 v or some wrong value.
At times when i connect multimeter to read volts across Capacitor , its reading gets correct .
am unable to understand the cause which is causing such wrong reading of cells and that too using EV2400 device.
Rohit