The TI E2E™ design support forums will undergo maintenance from July 11 to July 13. If you need design support during this time, open a new support request with our customer support center.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDA-00637: CT Part Number Used in TIDA-00637

Part Number: TIDA-00637

Hello E2E Experts,

Good day.

I have reviewed the documentation thoroughly, and I just wanted to confirm that in the document titled "Implementation of a Single-Phase Electronic Watt-Hour Meter Using MSP430F6736(A) (Rev. F)" (slaa517f.pdf), there is no mention of the accuracy class of the current transformer that is needed to achieve the Class 0.2 E-Meter rating. However, in "Level 1 and Level 2 Electric Vehicle Service Equipment (EVSE) Reference Design" (tidub87.pdf), which is the document that led me to slaa517.pdf, on page 18, it mentions that "An external 0.05% CT is required to meet the high accuracy specification with the appropriate burden resistor tuning." I just want to confirm that 0.05% is the intended number and not 0.5%. I ask because I have had significant difficulty finding a 2000:1 turn ratio current transformer with a 0.05% accuracy. If possible, can the part number of the current transformer used in the EVM for the single-phase meter be provided as a reference?

Thank you in advance.

Regards,

CSC