This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TIDA-00637
Hello E2E Experts,
Good day.
I have reviewed the documentation thoroughly, and I just wanted to confirm that in the document titled "Implementation of a Single-Phase Electronic Watt-Hour Meter Using MSP430F6736(A) (Rev. F)" (slaa517f.pdf), there is no mention of the accuracy class of the current transformer that is needed to achieve the Class 0.2 E-Meter rating. However, in "Level 1 and Level 2 Electric Vehicle Service Equipment (EVSE) Reference Design" (tidub87.pdf), which is the document that led me to slaa517.pdf, on page 18, it mentions that "An external 0.05% CT is required to meet the high accuracy specification with the appropriate burden resistor tuning." I just want to confirm that 0.05% is the intended number and not 0.5%. I ask because I have had significant difficulty finding a 2000:1 turn ratio current transformer with a 0.05% accuracy. If possible, can the part number of the current transformer used in the EVM for the single-phase meter be provided as a reference?
Thank you in advance.
Regards,
CSC
Hello CSC,
I will look into accuracy number of the CT and get back to you soon.
Best regards,
Errol
Hello Errol,
Good day.
Do we have the accuracy so far? I look forward to your response.
Regards,
CSC
Hi CSC,
Thank you for your patience, I was able to find the site where we acquired the CTs for the TIDA-010036 and TIDA-010037. TIDA-010037 is a Split-phase metrology reference design for electricity meters that meets ANSI C12.20 Class 0.1 active energy accuracy requirements across 10000:1 input range.
Which is achieved with ADS131M04 and MSP432 metrology library software calibration you can achieve accuracy. Attached below is the link to the CTs:
http://www.shenk.com.cn/proData.aspx?cateid=153&id=353
Best regards,
Errol
Hello Errol,
Good day.
Is it possible to use a different vendor? Are there alternatives? Is the accuracy 0.05% or 0.5%?
Also, I am using the MSP430F6736, so I am curious how applicable is the suggestion of an MSP432 solution.
Regards,
CSC
Hi CSC,
It is possible to use a different vendor. One alternative you could look at is Vacuumschmelze.
https://vacuumschmelze.com/products/Inductive-Components-and-Cores/Current-Transformers
The accuracy is 0.05% based on your initial inquiry. The MSP432 solution like TIDA-010036/37 are applicable and we have metrology software to implement the calculations.
This could be implemented on the new MSPM0 device family which can be a cost effective replacement MCU for MSP432 which implements the metrology calculations.
Best regards,
Errol
Hello Errol,
Good day.
I would like to highlight my inquiry below:
"Also, I am using the MSP430F6736, so I am curious how applicable is the suggestion of an MSP432 solution."
Regards,
CSC
Hi CSC,
I have looked at MSP430F6736 and this is an e-meter SoC. This can be replaced with a 2 chip solution using our ADS131M0x and MSPM0. That would be a cost effective solution in place of the MSP430F6736. One example of the 2 chip solution is TIDA-010037 which I have linked below.
https://www.ti.com/tool/TIDA-010237
Depending on the features needed we have a metrology library for basic metrology features working on the MSPM0 and the following library below that has worked on the MSP432.
https://www.ti.com/tool/ADC-ENERGY-METROLOGY-LIB-SW
Best regards,
Errol
Hello Errol,
Good day, and thank you for the additional information.
Hi CSC,
It took a while to find some with the accuracy requirements but have the following sensors:
High Accuracy Solid-Core Current Transformer - AcuCT S77 | Accuenergy
Hemeict - High Precision 0.05 Class Accuracy
top is 0.15% and bottom is 0.05%
Hope this help!
Best regards,
Errol