It is nice to have support for TPS61085 in SwitcherPro, but there is no possibility to change switching frequency from 1.2MHz to 650kHz. Even auto update is not working for me, because if I click to "Yes, download now", it act like instantly downloaded 100%, but in fact nothing is downloaded. Manual download is so difficult, because google can find download page faster than internal search. It is lot to improve, but I'm beliver.