This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDA-010086: How to perform discharge using TIDA-010086

Part Number: TIDA-010086
Other Parts Discussed in Thread: POWERSUITE

The TIDA-010086 mainly focuses on charging which is based on Buck conversion. I will need some pointers on how this reference design achieve CC and CV in details.

On top of that, a battery formation system will also include discharge operation. I believe the same circuit can be used for the operation but instead running a Boost converter from the perspective of the Battery terminal. 

I am trying to find more info on the boost in the  powerSUITE however there is no available example on boost converter. 

I would be glad if anyone could help on that

Thanks