This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PMP11107: Self-driven rectifier circuit in flyback designs (by D. Strasser)

Part Number: PMP11107
Other Parts Discussed in Thread: PMP11065

Hi,

in the flyback converter reference designs PMP11107 and PMP11065 the author implemented a self-driven secondary rectifier:

It works reasonably well in situations where one does not want to employ dedicated ICs. But I am struggling a little to fully understand the circuit. My musings so far:

  • In principle I think Q1 is used to quickly rush out the gate charge from Q2 to turn it off.
  • R7 limits the static base current of Q1 to some quiescent level, and C10 provides an AC path for a much higher current peak to speed up the switching of Q1.
  • D6 might be there to protect the base-emitter junction of Q1 from being excessively reverse-biased (might otherwise die at some 6V or so).
  • R5 and D4 then seem to provide the turn-on path for Q2.

Does that remotely make sense?

Thanks a lot & kind regards,

Sven