This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I'm trying to complete the PSpice for TI training Lab "16-1 Running Noise Analysis".
PSpice detected an imported model containing transistors or diodes after editing breakout.lib. Noise parameters cannot be selected in output window.
Since the transistor in the example is not available in the installed libraries, I edited the QbreakN part in the breakout.lib and replaced the transistors. However, I now receive the message: "PsPspice detected an imported model containing transistors or diodes". In addition I cannot select any noise parameters in the output window. I can't reverse the process by removing the parameters I added to the QbreakN model in the breaakout.lib
Basically, I want to be able to simulate a circuit containing a "non-TI" BJT and TI Op-Amps. Is that possible with the given limitations in Pspice for TI ?
Hi Michael,
Including non-TI transistor/diode models will trigger the soft landing that restricts the tool to 3 markers. You can still run the simulations, but will be limited in how many nodes you can monitor.
Not sure what's going on with the Noise sim. Let me check into that.
Likewise with removing the model changes. Seems like that should've canceled the soft landing.
I might need your zipped test bench to confirm all this, but let me see what I can find out first.
David
Hi Michael,
I'm not familiar with the noise analysis video 16-1.
Can you share that link?
I need your Project/Design so that I can see what's going on from my end. Otherwise, I'll just be guessing.
David
Hi David,
The PSpice for TI training Lab is downloaded from Cadence - https://www.pspice.com/pspice-for-ti/training-course
I did a fresh install on another machine where I could trigger/remove the TI soft landing by modifying the QbreakN model in Qbreakout.lib. I copied the breakout.lib and breakout.libsig to my first PSpice install and got that working as well.
When I trigger the TI soft landing (and have to put 1-3 markers on the schematic), the noise simulation output variables do no appear in the add traces window.
The following 2N2222 model were used for QbreakN:
+IS=3.88184e-14 BF=929.846 NF=1.10496 VAF=16.5003
+IKF=0.019539 ISE=1.0168e-11 NE=1.94752 BR=48.4545
+NR=1.07004 VAR=40.538 IKR=0.19539 ISC=1.0168e-11
+NC=4 RB=0.1 IRB=0.1 RBM=0.1
+RE=0.0001 RC=0.426673 XTB=0.1 XTI=1
+EG=1.05 CJE=2.23677e-11 VJE=0.582701 MJE=0.63466
+TF=4.06711e-10 XTF=3.92912 VTF=17712.6 ITF=0.4334
+CJC=2.23943e-11 VJC=0.576146 MJC=0.632796 XCJC=1
+FC=0.170253 CJS=0 VJS=0.75 MJS=0.5
+TR=1e-07 PTF=0 KF=0 AF=1
Example project is attached in zip
Hi Michael,
Thanks for pointing me to the training material. I had searched ti.com and pspice.com's training but didn't download this thinking it was just a repetition of other training.
I'm glad that you've got it working. It was confusing that when you went back to the original unmodified model it was still in soft landing.
Looks like you resolved that.
I'll check with Cadence on why the noise analysis is disabled during soft landing. It might be that the noise analysis requires monitoring many nodes that would violate the soft landing criteria. Alternatively, it's likely that some advanced features are disabled in soft landing to provide incentive to upgrade to the full version. If you are likely to be a heavy user of PSpice, then upgrading is probably the solution that you'll want.
Light or occasional users will be fine with PSpice for TI.
I'll play around with the project your supplied, but I don't think there's anything wrong. Just how soft landing and noise analysis interact.
David
Not sure why the tutorial says to monitor the bias circuit instead of the output. That's odd.
I'm not sure what you mean.
Bias for the Q1/Q2 current mirror is set by RBIAS.
V1 is source and differential output is out1/out2.
I had to re-read the module. I was surprised that they were looking at the noise contribution of the current mirror on the bias.
I did hear back about what's going on.
Noise analysis is not connected to markers. So if soft landing is triggered, without any markers, noise analysis won't work. This is true for the full version of PSpice as well (although there's no soft landing). just if no markers are selected, there won't be any Noise Analysis.
It's just how they implemented this feature.
David
I don't quite understand how this works.
With added markers appearing in the output plot, the noise output variable tick box is still greyed out in the "Add Trace" dialog box. The output window shows the "AC (and Noise) Analysis" ran.
When not in soft landing it is not necessary to add any markers to run "AC (and Noise) Analysis" and plot all noise variables.
This is how it looks in soft landing:
Hi Michael,
This is a bit of a black box. I'll ask for a clearer explanation and post that here if possible (unless it is proprietary).
David
Hi Michael,
Haven't heard back, but I think it's because you can have voltage or current markers, but there aren't any Noise markers.
So, when in soft landing, you are limited to 3 markers (current or voltage). Since there's no noise marker, you don't get noise analysis.
David
Hi David,
I guess you're right. It doesn't seems like noise simulation is an option in soft landing mode. I returned to LTSpice and got a simulation going of a circuit having models for BJT, OPA161x, OPAx206 and OPA1632 imported faily easy.
Michael