This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDA-010062: Test Setup for Labs

Part Number: TIDA-010062
Other Parts Discussed in Thread: PMP41006,

Hello,

To test the PMP41006 for 'Lab1' 

As mentioned in Section 3.1.1.3.2 of the design guide, the DC input voltage(upto 120V) is given at 'J7' for 'Lab' tests.

Need clarifications where exactly the 120VDC has to be applied? Since J7 will hold the for GaN daughter card.

Regards,