Other Parts Discussed in Thread: LMV431
Dear TI Team,
I have a query regarding the PMP8740 reference design. In the schematic file for the PMP8740 REVE 2kW BC Boost plus Aux Schematic, the VCC Primary is 12-12.5V in my design as well as in reference. I have replicated the same circuit, using identical parts and resistors with taking same tolerance, the measured Boodted DC Output voltage is "390V" during PFC boost. Without the boost, the output voltage is 338-339V(for 250VAC), and we expect to receive a status through the I/O. However, we are not getting the expected results; the I/O reads Low (PG_PFC is Pull up with 47k resistor to 5V) for both the normal and boosted DC voltage levels.
Could you please guide me on a solution to resolve this issue?I am seeking to achieve proper status indication for both voltage states through the I/O.
Thanks & Regards,
Meet Pandya