Other Parts Discussed in Thread: LM5069, LM7480
Hi,
My question relates MIL-STD-1275E Surge Protection Reference Design which using LM74800DRRRQ1 and LM5069MM-2 devices:
In the Design Guide TIDA-010242 is written "the output of the protection circuit should be nominal
28 V and maximum at 34 V" but nothing about the lowest VIN to operate properly.
In my application the used 24VDC input which may go down to 9V
Would this application schematic work properly when the input down to 9V?