Tool/software:
Hi,
We produced the TIDA-020047 reference design and we are facing issue related to PMIC which is not outputting the following voltages: 1.8V, 1.2V and 1.0V .
We checked the following test points and its OK:
- 12V exists at TP9
- 3.3V exists at TP42
But we didn't find voltages from PMIC output in J9 connector at:
- 1.8V at pin 1/4
- 1.2V at pin 7/10
- 1.0V at pin 25/28
We already pulled GPIO2 of PMIC to GND via 10K ohm resistor to trigger watchdog.
Could you help us to fix this issue is there any missing instructions that we should perform to make the PMIC outputting the needed voltages ?
Thanks.
Best regards.