This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM51551-Q1: LM51551-Q1 TINA simulation issue

Part Number: LM51551-Q1

Tool/software:

Hello,

I have made a power supply using LM51551-Q1 with Flyback configuration. I am simulating the circuit in TINA TI. The issue is IC is not producing any output. Don't know whether its a TINA TI simulator issue or something else.  The circuit is attached for reference.

Design parameters:

Input: 8V - 30V DC

Output: 12V/5A

Frequency: 100kHz