This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
When a single signal is connected to the op amp, there is no noise.
When two signals are connected to the op amp at the same time, the negative voltage is whistled.
Raising the frequency of the signal source or decreasing the amplitude can make the whistling disappear.
What is the cause of whistling, and what is the relationship between the frequency and amplitude of the whistling signal?
Hi Xie,
The Whistling noise could be due to multiple factors like inductor saturation, stability, pulse skipping frequency at audible frequency range. I recommend you to check the inductor selection, compensation components values.
Thanks,
Nitya