Part Number: UCC24624
Other Parts Discussed in Thread: UCC24612
Tool/software:
Hello,
I have been going through some other controllers for a synchronous rectifier such as UCC24612 and I noticed that they have calculations for the minimum RDS(ON) of the MOSFET (topic 8.2.2.1 from the datasheet). I am currently using the UCC24624 for a GAN FET (with body diode) that has an Rds(ON) of 0.7 mOhms. Can that restrict or limit how the UCC24624 controller works? I have noticed that the controller and the FETs are heating up when the power goes above 600 W. When the load is 1kW, the temperature of the controller is near 62 Celsius (not sure if that is normal).