I am designing a power supply using TPS54310 with the following specifications.
Vin (min) = 4.5V
Vin (max) = 5.5V
Vout = 1.875V
Iout = 0.8A
When I entered the above parameters, WeBench did not display TPS54310 in the list of recommended parts. I went on to investigate why not. It generated the following result (image attached). It says the “voltage is out of limit”. You can clearly observe that the voltage is in range. In fact I have implemented TPS54310 to generate the required supply too. I just wanted to check if I had the best balance of components. Is this is bug or am I interpreting something incorrectly?