Greetings,
Our customer pointed out a potential error in the LM3670. In the Webench interface it looks like the max output voltage is 2.5 where the datasheet and product page suggest the output voltage can be up to 3.3V. Is this the case for the adjustable version? It is not necessarily clear in the datasheet. For the adjustable version the datasheet only specs out feedback networks up to 2.5V.
Can you help clarify this?
Thanks, Tyler Pate