Other Parts Discussed in Thread: TPS40211, TPS40210
Hi, gentleman :
I try to use Switcher PRO to design my project. But I found the result of SwitcherPro is different to my calculation according to TPS40211's datasheet. For Example :
1. The output capacitance is 56uF, but the result of Switcher PRO is 470uF.
2. The power inductor L1 is 8.2uH, but the result of Switcher PRO is 1uH
I recognize the switching frequency is different with my case, but I believe these parameters don't have so large difference. Can you give me some tips ?
BR
Stone