How to generate this pulse train in tina with the above specification. This is used for clocking a register.
thanks and regards,
DHEERAJ
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
How to generate this pulse train in tina with the above specification. This is used for clocking a register.
thanks and regards,
DHEERAJ
Hi Dheeraj,
You can do that by placing a "Voltage Generator" from under "Sources" tab on the top. Attached is an example.
Best regards,
hi,
I have one more problem, I am working on ADC signals and the type of square wave generally obtained has rise and fall time of 10ns roughly and stable level time of 80ns, so in total 100ns ON time. The next sample comes after 50ms approx . For computational purpose I have to stretch the pulse. Hence I am using a peak detector circuit. Currently I am using OPA657N and 1N4148WT diode. The critical part is that the input signal amplitude varies from 100mV to 5 volts . So diode will be a problem in peak detector. It would be helpful if you could suggest me circuit or application specific opamp(part number).
DHEERAJ
Hi, you can detect the peak with the attached circuit, simulation is done with 100mV peak but works for lower voltages as well.
Regards,
Arash Loloee
SIR,
Please have a look at this circuit. I require an OP AMP based circuit. The sample input waveform is high speed. The duration is very less. I need to detect the input and then stretch the wave.
Thanks