This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
hello everybody please help me to simulate this program
V_V3 G N286413 DC 0 AC 0
G_G4 N286413 H VALUE { (1e-6)*VAL*PWR(EXPON,1) }
.PARAM ct3={5.862m} rt5={5.195m} ct4={1.093m} dfl30={0.2103} ct5={131.9u}
+ dfl20={0.8415} dfl31={-1.337m} dri30={4.064e001} dfl32={2.799e-006} dfl21=
+ {-5.510e-004} dfl10={1.000e-014} exposant=dri30 + (dri31 * v(t)) dfl11=1.603
--------------------------------------------$ ERROR(ORPSIM-16152): Invalid number
+ e-031 dfl22={-1.095e-006} dri20=2.737 e003 dri31=-0.1616 dri32=1.922e-4
+ dri21=-8.793 dri10=4.442 dfl12={-2.230e-034} dri11=-1.894 e-2 dri22=9.985e-3
+ expon=exp(pwr( v(a),2.1)/( dri20 + dri21*v(t) + dri22*pwr(v(t),2)))
+ dri12=2.642e-5 val=dri10 + dri11* v(t) + dri12*pwr(v(t),2) rt1={1.979e-1}
+ drq10={-6.658e-002} rt2={7.750e-002} drq11={8.592e-001} ct1={0.1141} rt3=
+ {1.591e-001} drq12={-6.884e-003} rt4={2.304e-002} ct2={7.395e-002}
.subckt SCHEMATIC1_Reset 1 2 3 4
S_Reset 3 4 1 2 _Reset
RS_Reset 1 2 1G
.MODEL _Reset VSWITCH Roff=1e6 Ron=0.1 Voff=1 Von=0
.ends SCHEMATIC1_Reset
Karim,
We will need a lot more information to help. What are you trying to simulate? What simulator are you using? Where did the model/netlist you are using come from? Is there more than just this section of the netlist?
This kind of information is essential to finding out what the error means and what has caused it.
Britt