This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Greetings,I am having a trouble with the WEBENCH designer that everytime i have designed the ckt of lm2678-adj and wants to export the cad file,the cad file doesn't seem to open in either Eagle or Orcad.
The steps mentioned in the readme file are strictly followed yet sometimes in Eagle file board file is missing and in Orcad it doesn't verifies the .edf file.
Please try to resolve this issue and let me know if their is any other solution
Hi,
Can you please post both the Eagle and Orcad exported zipped files so we can trouble shoot the issue?
I was able to import this design into ORCAD CIS, please open attached by clicking the 2014-11-02_06-05-01.opj project file and let me know if any other issues.
Regards, Mike1537.Orcad.zip
I have confirmed the issue.
There are problems exporting CUSTOM components into Eagle.
Please try to select an alternate component for L1.
Apologies for the inconvenience, we are working on a solution for exporting CUSTOM components into Eagle.
Regards, Mike
ok, so i downloaded the zip file and tried to open it via Orcad Capture CIS Version 9.2 but it is giving an error.
ERROR [DBO3220] Attempt to read file with invalid file format
What version are you using?
thanks for the prompt reply.
As i am avid user of orcad, i would highly recommend the orcad issue to be resolved or a solution guided to me.
In other case, i would try to use Eagle if issue cannot be solved asap.
I am using ORCAD CIS v16.5.
I have tried saving again to earlier compatible format, please try opening the v16_2.opj (apparently there was a change in the dsn file format from v16.3 onwards).
Regards, Mike
Hi Andreson,
Can you please try once more using the attached file to see if it can be opened with version 16.2? I converted the file using version 16.3.
Sorry, as i told you before i only have version 9.2 so all your files are not opening on it.