Other Parts Discussed in Thread: LM3478
Hello,
I need some help for the LM3478. I'm using this device to build a Step Up converter with the following specs: V input = 4,8-6 VDC and V out = 60VDC, 0.25A. The circuit according to the Webench is the following one
but I don't get 60V in the output, I get around 6.5V...
So, I decided to make some changes to the circuit according to the LM3478 data sheet. You can see them in the picture above.
I used these schematics as a reference.
I calculated that the inductor can be from 1uH to 10uH depending on the switching frequency.
After these changes, my new output is 8.6V (still far much lower than the desirable 60V). What am I doing wrong? I would appreciate any help!
Best regards,
Sotirios Gakopoulos