This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

tps54240, tps62133 transient models apparently not working on buck-boost inverting configuration

Other Parts Discussed in Thread: TPS54240, LM43602, LM46001, LM46000, LM46002, LM43603, LM43600, LM43601

as the title says the model doesn't work as expected

using the reference design provided by the datasheet

http://www.ti.com/lit/ds/symlink/tps62133.pdf\


now when running the simulation something quite strange happens, the inverted voltage stays put, it never decreases with time (i know the diode is in an awkward position and that it should go before the inductor in a normal inverting buck boost, just following the reference, if setting the diode before the inductor the device wont switch in the simulation)

something similar happens with the tps54240 (this one in the normal buck-boost configuration) i've built an inverting converter with a tps54240, and it worked as expected

should it be that these models aren't expected to work in this configuration or am i doing something wrong?