This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS62090 - Webench simulation data(Vin=5V, Vout=1V, Iout=3.0A) and switching frequency(Fs)

Other Parts Discussed in Thread: TPS62090

Hi all

Would you mind if we ask TPS62090?

Our customer will use TPS62090 as following conditions;
-Vin : 5V
-Vout : 1V
-Iout : 3A
-Fsw : 2.8MHz(FREQ pin connects to GND)

<Question1>
When we simulate above conditions of  Vin, Vout and Iout, we could not simulate.
Then, it showed the message "For Vout<0.6V, current limit of 1.5A is being exceeded for the given design condtions during startup." on pop-up window "Parts Not Found". Please refer to the attached file.
3644.20151023_TPS62090_Webench simulation.pdf
So, is it possible to achieve above condtions? or not?

<Question2>
We could not find out the switching frequency on the datasheet P6 at above conditions;
It will be approximate 2.2 MHz, won't it?

Kind regards,

Hirotaka Matsumoto