Hello,
I started looking into the LM536003 as an option for a 3.3V source. The Webench circuit looked pretty simple, so I download the encrypted PSpice model to start working with it for my application. I'm having convergence issues that I can't get passed.
I need an input ripple filter on the design, so I had Webench add in it's calculated version. If I run the example Startup Transient simulation included as an example in the PSpice model package, it runs as advertised. If I add in any resistance to Vin (either as an equivalent impedance using an inductor or as part of the input ripple filter) then the simulation fails to converge. At this point no combination of tricks I know for improving convergence in PSpice has worked.
If you want to try creating this, the only components added to the packaged example are for the input ripple filter: a 4.7u cap (3 mohm ESR, Cf_inpflt), a 120 nH inductor (86 mohm DCR, Lf_inpflt), a 100 mohm resistor (Rd_inpflt), and a 22u cap (80 mohm ESR, Cb_inpflt).
This is the convergence error from the provided example when run with the input filter, all are internal to the LM536003 (U1) with the exception of the voltage source (V2). The convergence issue appears at about the time soft start would end:
ERROR(ORPSIM-15138): Convergence problem in Transient Analysis at Time = 3.604E-03.
Time step = 596.3E-21, minimum allowable step size = 1.000E-18
These voltages failed to converge:
V(X_U1.U4_N08977) = -31.25mV \ 7.813mV
V(X_U1.U4_N08957) = -17.35mV \ 303.25uV
V(X_C1._SR) = -1.986mV \ -608.51uV
These supply currents failed to converge:
I(X_U1.E_U7_ABM3) = 976.88uA \ 488.60uA
I(X_U1.E_U2_E2) = -51.81nA \ 14.47nA
I(V_V2) = 0A \ 3.906mA
I(X_U1.V_U4_V8) = 974.98pA \ -622.09pA
I(X_U1.V_U4_V7) = -964.25pA \ 623.69pA
I(X_U1.V_U1_V6) = 947.65pA \ -615.42pA
I(X_U1.X_U4_H2.VH_U4_H2) = 17.35mA \ -303.25uA
I(X_U1.X_U4_H1.VH_U4_H1) = -31.25mA \ 7.813mA
I(X_U1.X_U4_H2.H_U4_H2) = 17.35mA \ -303.25uA
I(X_U1.X_U4_H1.H_U4_H1) = 31.25mA \ -7.813mA
Thanks for any help or ideas to get past this.
Lenny